A GATEWAY report on a trial demonstration has been released by The U.S. Department of Energy (DOE) in which quartz metal halide (QMH) area lighting was replaced with LED products at three pole locations along a 7.2-mile stretch of the Yuma, Arizona’s Sector Border Patrol Area. The LED system was found to equal or better the incumbent system in terms of both luminance and uniformity, and an advanced optical system and lower pole height improved the luminance uniformity, reduced stray light, and increased projected energy and maintenance cost savings. The high-luminous-flux and high-temperature application is not unique and similar applications can benefit from the findings including correctional facilities, military bases and common street and area lighting.
With the goal to help local governments cut their outdoor lighting bills by 50 percent or more, the U.S. Department of Energy announced the launching of the Presidential Challenge for Advanced Outdoor Lighting, and has tripled the DOE Better Buildings program goal of upgrading 500,000 poles to 1.5 million. Why? Communities are installing LEDs, and showcasing market acceptance and satisfaction with the technology. Some communities are showing even greater energy savings — as much as 70 percent more with lighting controls.
Eaton’s ARRA Controls Solutions website page has been updated with new information explaining the difference between the Buy America Act, Buy American Act, as well as the American Recovery and Reinvestment Act (ARRA). This page also has an updated list of controls products that currently help comply with these provisions.
The new Night Falcon LED floodlight combines superior illumination with advanced engineering design to deliver significant energy savings at a fraction of the cost of traditional HID products. Check out the Night Falcon video and web page to learn more.
Delivering unparalleled uniformity and budget-conscious operating costs, the roadway, area/site luminaire is offered in three optical distributions and lumen packages up to 8,500 to replace up to 150W HPS fixtures.
The 865 sconce is available in 14- and 18-inch diameters, four color temperatures and in a variety of metal and painted finishes. The ADA complaint sconce features a timeless geometric shape with companion pendants available.
The 8-inch LED cylinder line has added 8,000 and 9,000 lumen options, easily replacing 500W quartz and high wattage HID products. They’re designed for easy installation in pendant, surface- or wall-mounted applications, providing energy-efficient, glare free illumination.
Designed to allow ambient recessed products to mount in surface-mounted application, these universal surface kits fit 2' x 2' and 2' x 4' LED and fluorescent recessed troffers to accommodate Metalux, Fail-Safe, Corelite, Neo-Ray and other compatible products.
The round LED low bay luminaires feature WaveStream™ LED technology, offering a precise combination of vertical and horizontal distribution available in both medium and wide distributions – ideal for auditoriums, retail, big box, airports and municipal applications.
Check out our Halo RL56 and RA56 LED Downlights being featured on Hometime (episode 2826) with Dean Johnson. The products were installed in the Creekside Home project. Hometime is one of the longest-running home improvement programs on television, airing for 27 years on PBS and 12 years in commercial syndication.
The Metalux LED Encounter, Corelite Divide LED Suspended Pendant and the McGraw-Edison TopTier LED Parking Garage Luminaire were recognized with Silver honors in the IIDEXCanada Innovation Awards, which celebrates the latest and most innovative product designs and is organized by Interior Designers of Canada (IDCanada).
The Galleon LED Area/Site Luminaire from Eaton’s Cooper Lighting business has been selected a winner in the fifth annual Architectural SSL magazine Production Innovation Awards (PIA). The awards program honors the most innovative LED luminaires and fixtures on the market, while also recognizing the companies behind the components that make up these light sources.
LEDs Magazine has named four Eaton lighting products as finalists in its inaugural Sapphire Awards program. The program selects the very best in LED technology.
Indoor SSL Luminaire Design
Neo-Ray Index LED Pendant
Halo SLD Surface LED Downlights
Industrial SSL Luminaire Design
Metalux SkyBar High Bay Luminaire
Outdoor SSL Luminaire Design
McGraw-Edison TopTier LED Parking Garage Luminaire
http://iesrmsdenver.org/2014/10/rocky-mountain-lights-march-19th/
http://www.iesna-mi.org/index.htm
http://techomebuilder.com/summit/
Peachtree City, GA
Peachtree City, GA